Loading
Blog
Recent ActivityRecent Activity

Introduction to Containerization: Bridging IT and OT

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Man and woman using FactoryTalk Optix as their HMI solution.

Containerization is a virtualization technique that has existed since at least 2008. It is a type of software deployment that bundles together everything needed to run in a single package. This includes an application and all its dependencies. While historically it’s been used in IT environments, it has recently been gaining traction in OT. Modern containerization, popularized by Docker® since 2013, enables efficient, portable application deployment across diverse environments. Industry standards focusing on user experience with containerization have been formed by the Open Container Initiative (OCI). Containerization gives the ability to run applications that would have otherwise been limited by device or operating system. The goal of this post is to demonstrate containerization’s power to streamline application deployment across IT and OT environments, transforming efficiency in modern Industrial Control Systems (ICS).

Containers vs. Virtual Machines

The easiest comparison with containers is virtual machines (VMs), as both are types of virtualizations. A key difference is that containers don’t require an entire Guest Operating System to run, while VMs do and virtualize everything down to the abstract physical layer. VMs demand significant CPU and memory, limiting scalability in resource-constrained settings. Containers share the host OS kernel, making them lightweight and fast, with startup times in seconds compared to minutes for VMs. This efficiency stems from packaging only the application, libraries, and configurations. For example, a containerized app runs identically on a developer’s laptop or a cloud server, ensuring consistency across development, testing, and most importantly for industrial control systems: production.

Graphic comparing virtual machines to containerization
FactoryTalk Optix
FactoryTalk Optix
FactoryTalk Optix
Achieve your HMI, IIoT, Edge and Data Platform vision with collaboration, scalability and interoperability that improve deliverables and efficiency.
Learn More
Containerized software solves IT & OT integration
Containerized software solves IT & OT integration
Blog
Blog
Containerized software solves IT & OT integration
Engineers can bridge IT and OT. Containerized software reduces environment drift and improves consistency from development to production across IT & OT
Read Now

Infrastructure: The physical hardware, such as servers, storage, and networking equipment, that provides the foundational resources for virtualization.

Host OS: The primary operating system installed directly on the physical hardware, managing resources and running the hypervisor.  

Hypervisor: A software layer that creates and manages virtual machines, allocating resources between the host and guest operating systems. 

Guest OS: An operating system running within a virtual machine, isolated from the host OS, used to execute applications. It relies on the hypervisor for access to virtualized hardware resources.

Containers in Industrial Control Systems

A key benefit to containers, especially in the ICS space, is the amount of space that a container requires—as Industrial Internet of Things (IIOT) devices typically have smaller amounts of memory and less processing power. Containers can be important for ICS systems as they are so lightweight and flexible that they can be used by many IIOT devices. In ICS, containers enable edge computing for real-time analytics, such as monitoring SCADA systems or processing sensor data on IIoT devices. Containers also support OT-IT convergence by enabling consistent deployments across hybrid environments.

Additionally, containers offer scalability, allowing deployment of lightweight services on small edge devices or larger, orchestrated setups on server clusters, supporting distributed architectures from edge to cloud. Compatibility is enhanced since containers bundle dependencies, simplifying installation and ensuring consistent execution across diverse environments without dependency conflicts. Security is also improved, as containers can be built following published best practices, requiring authentication for deployment to runtime hosts without needing administrative privileges, unlike traditional software installations on Windows systems. Containers also enable quick recovery and migration, facilitating rapid upgrades or system restoration by redeploying containerized applications with minimal downtime. Finally, containers are here for the foreseeable future, since they align with modern IT development trends, ensuring ICS systems remain adaptable to evolving technological demands.

An example of using containers at Rockwell Automation has been in the FactoryTalk® line. FactoryTalk Analytics GuardianAI is only delivered in a container. It is an application that can run predictive maintenance algorithms on a factory floor edge device, using minimal resources and needing no coding skills.

ThinManager® and FactoryTalk® Optix™  

Another containerized solution has been recently added to the FactoryTalk line. It is now possible to deploy a FactoryTalk Optix Application Container with ThinManager in versions 1.6 and 14.1 respectively. FactoryTalk Optix is a software platform that enhances HMI and data visualization experience and augments capabilities in edge computing and data management. ThinManager devices use thin clients (devices with lightweight hardware and little-to-no OS requirements) to simplify Industrial Control Systems in part by running containers. This means it’s possible for the infrastructure requirements of an HMI to be significantly reduced. ThinManager’s centralized management allows for scalable, consistent deployment, minimizing hardware costs and simplifying updates, while enhancing security. A more thorough breakdown can be found in this video or in a future dedicated post.

Merge Best IT Practices and OT Realities
Merge Best IT Practices and OT Realities
Blog
Blog
Merge Best IT Practices and OT Realities
Software containers on the Edge deliver: 1. Fast Deployment 2. Customization 3. Resource Efficiency 4. More Security 5. Simplify Management 6. Scalability
Read Now
Streamline OT with Containerized Software: 5 Ways
Streamline OT with Containerized Software: 5 Ways
Blog
Blog
Streamline OT with Containerized Software: 5 Ways
Containerized software address 5 OT issues – See how it helps provide scalable, secure control that simplifies operations and empowers your team.
Read Now

Published August 6, 2025

Topics: Optimize Production Accelerate Digital Transformation Human Machine Interface Digital Transformation Human Machine Interface FactoryTalk Analytics GuardianAI ThinManager FactoryTalk Optix

Rylee Domonkos
Rylee Domonkos
Intelligent Devices/Software & Control Leadership Development Program Associate, Rockwell Automation
Rylee is a Leadership Development Program associate currently working in business strategy and product management at Rockwell Automation. Rylee is focused on the adoption of containerized solutions in Industrial Control Systems, simplifying product deployment and enhancing knowledge for OT customers.
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Introduction to Containerization: Bridging IT and OT
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose