Downloads
What does this application do?
This application serves as an example of how to use the raM_Tec_RotaryKnife library.
This AOI calculates four cam profiles for the rotary knife:
- Connection cam for acceleration from a stationary position. Typically from the initial axis position after homing or when there is no product/bag in production.
- Cyclic cam for continuous motion: one cut per product length.
- Disconnection cam for deceleration when stopping the knife without stopping the master axis.
- Dwell cam to keep the slave axis stopped for one product length.
When to Use: When a rotary knife cam profile is required for an axis.
When NOT to use: Not applicable (NA).
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
Functional Description
The cam calculation instruction generates profiles to synchronize the knife speed with the conveyor while they are in contact.
During the cyclic operation of a rotary knife, there is a synchronized portion and a compensation portion (see image below). The synchronized portion ensures that the knife and conveyor speeds are equal, while the compensation motion allows cut lengths to be shorter or longer than the circumference of the knife roll by accelerating or decelerating.
How can I make it work?
Requirements: products, tools, prior knowledge.
Hardware
- CompactLogix 5380
- Kit Kinetix 5500
Software
- Studio 5000 - Version 35
Relevant links (internal or external)
- Download the libraries on the following link: https://compatibility.rockwellautomation.com/Pages/MultiProductFindDownloads.aspx?crumb=112&mode=3&refSoft=1&versions=56336
Implementation Guide
- Step 1
- Step 2
- Step 3
- Step 4
- Step 5
- Step 6
5.1 - Now go to the Ram_LD_RotaryKnife routine and configure the AOI according to your requirements.
rotary-knife_Step5-1.png
This is an example of how to configure a cam for a rotary knife in the Add-On Instruction (AOI).
5.2 - After homing, the knife is positioned 180 degrees away from the cutting position, and the film position is 200 units away from the first cut.
- There is only one knife in the jaws.
- The knife radius in the jaws is 50 mm.
- After homing, the knife position is 180 degrees from the cutting position.
- After homing, the film position is at the center of the product.
- The cutting angle is 60 degrees.
- The product length is 400 mm.
- When the knife stops, it is intended to stop exactly at the same position as after homing (so that it can start using the connection cam when there is no product/bag in operation).
rotary-knife_Step5-2.png
Rotary Knife
Version 1.1 - May 2026