Limitations and Disadvantages
- Software must be updated to the latest versions.
- LOGIX control platform with MOTION capability is required.
This application demonstrates an integrated solution for the movement of independent carts using iTRAK, Logix control, and visualization with FactoryTalk Optix. It enables the simulation and validation of high-performance architectures, delivering flexibility, synchronization, and precision in transport. It serves as a practical reference for customers to understand gains in productivity, scalability, and the reduction of traditional mechanical systems. It also accelerates the development of real projects by providing an environment ready for testing, learning, and replication.
An application that demonstrates the control and synchronization of independent carts with iTRAK, using Logix and FactoryTalk Optix for operation and diagnostics. It enables the validation of flexible and scalable architectures, highlighting productivity gains and reduced mechanical complexity in industrial transport systems.
Limitations and Disadvantages
Downloads
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
How can I make it work?
Requirements: products, tools, prior knowledge.