Loading
Innovation Center LOGO
Recent ActivityRecent Activity

Export Report Variables from FactoryTalk Optix

Step-by-step process for generating PDF reports of process variables from the simulated operation of an electric motor. Additionally, this application provides a framework for building a first application in FT Optix. - [Implementation time: 30 Minutes]
Innovation Center Home Page
Corporate Analyst Reviews Digital Compliance Logs Thoroughly
Innovation Center LOGO
  • Overview
  • Installation Guide
  • Downloads
  • Contact us
  • I want to subscribe.
Innovation Center Home Page
 

What is this for?

The native generation of PDF reports without coding in FactoryTalk Optix enables automated digitalization of production, audit, and quality control data directly at the Edge. This function is critical for traceability compliance, allowing operators to export summaries of alarms, trends, and historical variables with a single click into a PDF file.

Additionally, the FT Optix application provides a reference framework for building your first FT Optix application.

 

Is this useful to me?

This is useful for users who have questions about how to create their first FT Optix projects, as well as for generating reports of process variables logged remotely from any database.

 

Application areas: Any type of industry that requires variable logging.
 

AHIC Download ICON VF.png

Downloads

Please note: You will need to agree to the Terms & Conditions for each download.

Downloadable file ›
Legal Disclaimer Acceptance. ROCKWELL AUTOMATION WILL PROVIDE ACCESS TO ROCKWELL PRODUCTS (BEST PRACTICES, APPLICATIONS AND KNOWLEDGE) ON THE CONDITION THAT YOU ACCEPT AND COMPLY WITH THE FOLLOWING TERMS AND CONDITIONS. YOU ACCEPT AND AGREE TO BE BOUND BY THE TERMS OF THIS AGREEMENT BY DOWNLOADING, INSTALLING, COPYING, OR OTHERWISE USING PRODUCTS. IF YOU ARE ACCEPTING THESE TERMS ON BEHALF OF ANOTHER PERSON, COMPANY, OR OTHER LEGAL ENTITY, YOU REPRESENT AND WARRANT THAT YOU HAVE FULL AUTHORITY TO BIND THAT PERSON, COMPANY, OR LEGAL ENTITY TO THESE TERMS. IF YOU DO NOT AGREE TO THESE TERMS, DO NOT DOWNLOAD, INSTALL, COPY, ACCESS, OR USE THE PRODUCTS, SOFTWARE AND/OR CLOUD SERVICES. 1. Rockwell Automation retains full ownership and title to all Products and related documentation. No rights or licenses are granted other than those set forth in this Agreement. Company grants to Rockwell Automation a non-exclusive, worldwide, royalty-free, perpetual, non-revocable license to use any feedback Company provides regarding the Products, even if Company has designated the feedback as confidential. Rockwell Automation will be entitled to use the feedback without restriction or compensation to Company. 2. Company may not lease sub-lease, assign, license, sub-license or otherwise transfer any of the Products without the prior written consent of Rockwell Automation. Company may not assign or otherwise transfer access rights to the Products without the prior written consent of Rockwell Automation. Any reverse assembly, reverse engineering, decompilation, and creation of derivative works based on the Products by Company is prohibited. 3. Company acknowledges that Products provided under this Agreement are Rockwell Automation’s Confidential Information and are covered by effective or pending copyrights, patents, trademarks and/or trade secrets of Rockwell Automation, and Company agrees to maintain confidentiality by not disclosing Products or documentation to any third party without the prior written consent of Rockwell Automation and to protect the confidentiality of the Products as it would Company’s own confidential information. Company agrees that its obligation of confidentiality under this paragraph shall survive expiration or termination of this Agreement. 4. Company agrees that Products provided under this Agreement are prototypes and examples and its application and results may vary depending on each customer and project conditions. Rockwell Automation do not warranty the same results. This Agreement shall in no way be construed as a commitment by Rockwell Automation at any time to manufacture and/or offer Products for sale. There is no explicit or implicit service level agreement associated with using the Products. Rockwell Automation does not warrant that the functions contained in the Products will meet Company’s requirements. Company agrees to use all Products only in accordance with the instructions and only for the intended usages identified in the documentation. 5. EXCLUSION OF WARRANTIES AND LIMITATION OF LIABILITY. THE PRODUCTS ARE PROVIDED "AS IS". ROCKWELL AUTOMATION DISCLAIMS ANY AND ALL WARRANTIES, EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE. ROCKWELL AUTOMATION EXPLICITLY DISCLAIMS ALL WARRANTIES OF NON- INFRINGEMENT AND EXPRESSLY DOES NOT WARRANT THAT THE PRODUCTS, IN WHOLE OR IN PART, WILL BE ERROR FREE OR FREE FROM SECURITY VULNERABILITIES. IN NO EVENT SHALL ROCKWELL AUTOMATION BE LIABLE FOR (i) LOST PROFITS, LOST SAVINGS, DOWNTIME, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES OF ANY KIND, OR (ii) ANY PERSONAL INJURY, PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE ARISING OUT OF OR IN CONNECTION WITH THIS AGREEMENT, WHETHER IN AN ACTION IN CONTRACT, STRICT LIABILITY OR IN TORT INCLUDING NEGLIGENCE. 6. COMPANY AGREES TO INDEMNIFY AND HOLD ROCKWELL AUTOMATION HARMLESS FROM ALL COSTS, AWARDS, DAMAGES, EXPENSES AND FEES (INCLUDING ATTORNEYS FEES) RESULTING FROM OR RELATED TO ANY THIRD-PARTY CLAIMS (INCLUDING EMPLOYEES AND AGENTS OF COMPANY) AGAINST ROCKWELL AUTOMATION, ITS DISTRIBUTORS, AGENTS, OFFICERS, DIRECTORS OR EMPLOYEES FOR PERSONAL INJURY (INCLUDING DEATH), PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE RELATED TO OR RESULTING FROM THE USE OF THE PRODUCTS. 7. In the event a Product is exported, Company agrees to comply with all applicable United States Export Control Law and Regulations, and the applicable export control laws of other countries. This Agreement shall be governed by the laws of the state of Wisconsin. This Agreement is the complete and exclusive Agreement between Rockwell Automation and the Company, and supersedes all prior agreements, whether written or oral, relating to the Products.
AHIC NEED HELP ICON VF.png

Need Help?

If you need help with an application or have feedback from the Innovation Center, please contact us.

 

How can I make it work?

  • Hardware
    • Personal computer
  • Software
    • FactoryTalk Optix
    • Studio 5000
    • FT Echo
  • Background knowledge 
    • Knowledge of programming and configuration in FT Optix and Studio 5000.
 
 
 
 
 
 
 
 
AHIC STEP ICON.png

Implementation Guide

 
  1. Step 1
  2. Step 2
  3. Step 3
  4. Step 4
Open All Close All
Step 1
 

Glossary of Object Concepts in FactoryTalk Optix

To better understand the objects used in the application, it is recommended to understand their meaning.

  • Navigation Panel - A user interface (UI) component designed to manage navigation between different application screens. It allows switching visual containers in an automated and structured manner using native events, enabling efficient and intuitive workflows for the operator without overloading the rendering thread.
  • Panel (Type) - A base visual node that acts as a general-purpose container in the user interface. As it is treated as a Type, it allows inheritance, mass instantiation, and the creation of custom templates (widgets). It can host local logic, variable collections, or complex layouts, serving as a modular building block of the interface.
  • DataGrid - An advanced tabular visual component designed for real-time visualization and editing of large volumes of structured data (such as database records, controller arrays, or alarm lists). It supports dynamic binding to data models (Model) and direct interaction with rows/columns exposed as objects within the session information model.
  • GridLayout - A UI layout control that automatically organizes its child nodes into a two-dimensional matrix structure of flexible or fixed-size rows and columns. It optimizes High-Performance HMI design, ensuring that diagnostic visual elements maintain consistent proportions and strict alignment when screen resolution changes or during remote web access.
  • Data Logger - A core module of FactoryTalk Optix responsible for sampling, storing, and transferring historical process and status variables into a data store. It supports time-based (periodic) or event-based (change-of-state) triggers, natively translating controller tags into relational structures compatible with IT systems.
  • Datalog Embedded - A specific storage engine configuration in which the history collected by the Data Logger is directly written to a local runtime database based on SQLite technology. This solution does not require external servers, making it ideal for Edge applications or closed devices such as OptixPanel, operating efficiently within the token-based licensing model (included with Data Logger).
  • Reports - A native component and rendering engine responsible for automated generation and export of reports in PDF format based on visual design templates (UI). It allows associating model variables and dynamic SQL queries directly with the final document for audit, quality control, and regulatory compliance (such as CFR21 Part 11).
     
Step 2
 
Model Configuration (Studio)

To create and configure a PDF report using the native functions and interconnections of the Information Model in FactoryTalk Optix Studio, follow these steps:

  • Instantiate the Reports Engine and Visual Template
  • In the Project Panel, expand the main project node.
  • Right-click the Reports folder (or project root) and select New -> Report. A new node will be created acting as the report generation engine. Name it Reports1.
  • When creating the report, a visual container is automatically added under the UI folder: Navigate to UI -> Reports  and locate the associated visual panel (usually named Reports1)
  • This is the report template.
  • Double-click the panel to open the graphical editor. Design the report layout using High-Performance HMI guidelines.

Example: Insert a Label object in the header for the report title (e.g., "OEM Company Buenos Aires, Argentina")
 

export-report-variables-from-factorytalk-optix_Image 1.jpg

export-report-variables-from-factorytalk-optix_Image 1.jpg

  • In the Sections area, insert a DataGrid component to display historical tabular data.
export-report-variables-from-factorytalk-optix_Image 2.jpg

export-report-variables-from-factorytalk-optix_Image 2.jpg

Step 3
 

Bind Data to the Report (Native Data Binding)

  • Select the DataGrid component in the report template.
  • In the Properties panel, locate the Model property.
  • Click the Dynamic Link icon.
  • Navigate in the Information Model to the historical data source, for example: Model/DataLoggers/PlantDataLogger/DatalogEmbedded
  • The component will automatically map database columns (timestamps, process variables, states) into the report view.
     
 

Configure the Generation Trigger in the UI and PDF Output Parameters

  • Go to UI -> MainWindow (Type)
  • Add a Panel (Type) called Report (Type) where the print button will be placed.
  • Insert a Button component and rename it:"Generate PDF Report"
  • Select the button and go to Properties -> Events
  • In the MouseClick event:
    • Click + to add a new action
    • Select ExecuteMethod
  • In the Method field:
    • Navigate to Reports -> Reports1
    • Select the method GeneratePdf

OutputPath
Define the output file path and name. To make it dynamic and platform-independent (Windows/Linux/OptixPanel), use: /Ruta/MotorStatusReport.pdf
 

export-report-variables-from-factorytalk-optix_Image 3.jpg

export-report-variables-from-factorytalk-optix_Image 3.jpg

Step 4
 

Run the FT Optix Emulator and Tes

Run the FT Optix emulator

• Connect it to FT Echo and Studio 5000
• Modify some motor variables
• Press the button to generate the report

Result
The application will generate a PDF report that includes:
• Timestamp
• Actual speed
• Setpoint
• Voltage
• Motor state
 

export-report-variables-from-factorytalk-optix_Image 4.jpg

export-report-variables-from-factorytalk-optix_Image 4.jpg

export-report-variables-from-factorytalk-optix_Image 5.jpg

export-report-variables-from-factorytalk-optix_Image 5.jpg

export-report-variables-from-factorytalk-optix_Image 6.jpg

export-report-variables-from-factorytalk-optix_Image 6.jpg

export-report-variables-from-factorytalk-optix_Image 1.jpg

export-report-variables-from-factorytalk-optix_Image 1.jpg

export-report-variables-from-factorytalk-optix_Image 2.jpg

export-report-variables-from-factorytalk-optix_Image 2.jpg

export-report-variables-from-factorytalk-optix_Image 3.jpg

export-report-variables-from-factorytalk-optix_Image 3.jpg

export-report-variables-from-factorytalk-optix_Image 4.jpg

export-report-variables-from-factorytalk-optix_Image 4.jpg

export-report-variables-from-factorytalk-optix_Image 5.jpg

export-report-variables-from-factorytalk-optix_Image 5.jpg

export-report-variables-from-factorytalk-optix_Image 6.jpg

export-report-variables-from-factorytalk-optix_Image 6.jpg

 
 
 
 
 
 
 

Export Report Variables from FactoryTalk Optix

Version 1.0 - June 2026

 

 
 
AHIC White Logo
Subscribe!

Receive new app releases and other updates from the Innovation Center directly in your inbox.

I want to subscribe.
 
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Sup...
  3. Chevron LeftChevron Left Pro...
  4. Chevron LeftChevron Left Downloads
  5. Chevron LeftChevron Left Innovation Center
  6. Chevron LeftChevron Left Export Report Variables from FactoryTalk Optix