Downloads
What does this application do?
The Connected Plant Monitor application is a demonstration project built in FactoryTalk Optix that shows how industrial data can be collected and visualized using the MQTT communication protocol. The Connected Plant Monitor application is used to collect, consolidate, and visualize real-time and historical industrial data transmitted via MQTT from one or more field applications, providing a centralized dashboard for monitoring plant or machine information.
- General Features
- Advantages
- Limitations/Disadvantages
The main features to the Connected Plant Monitor application are:
- MQTT-based communication between industrial applications using a Publisher/Subscriber architecture.
- Collection of real-time (live) data from field devices or machine applications.
- Collection of historical data from dataloggers and event logs.
- Dashboard visualization of received operational data.
- MQTT Subscriber functionality to receive information published by the MQTT_Field application.
- Support for custom MQTT messages through configurable payload topics.
- Monitoring of connection status through indicators such as connection state and Live Data LED.
- Reception of alarm and event information in addition to process values.
- Store-and-forward capabilities for transferring historical records through MQTT topics.
- Support for multiple machines or production sites through configurable table prefixes, allowing data source identification.
- Built with FactoryTalk Optix using Runtime NetLogic components for MQTT data exchange.
The Connected Plant Monitor application provides several advantages for industrial monitoring and IIoT implementations:
- Centralized data visualization through a single dashboard that consolidates information from machines and production systems.
- Real-time monitoring by receiving live MQTT data with minimal latency.
- Scalability, as multiple machines or production sites can publish data to the same MQTT infrastructure.
- Demonstration MQTT broker. The example uses the public broker test.mosquitto.org, which is intended only for demonstration purposes and does not guarantee availability, security, or performance.
- No built-in enterprise historian. The example demonstrates MQTT data forwarding and visualization but does not provide the advanced capabilities of dedicated industrial historians such as long-term archiving, compression, redundancy, or enterprise analytics.
- Dependent on MQTT infrastructure. Communication reliability depends on broker availability, network connectivity, topic configuration, and QoS settings.
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
Is this application relevant to me?
- Integrate multiple machines or sites into a centralized dashboard using MQTT topics.
- Build proof-of-value (POV) projects showing real-time and historical data aggregation from machines or production lines.
- Demonstrate MQTT communications between industrial assets and supervisory applications.
Application areas:
- Food & Beverage, Discrete Manufacturing, OEMs (Machine Builders)
- IIoT and Digital Transformation Projects
- Multi-Machine and Multi-Site Monitoring
- Remote Equipment Monitoring
How can I make it work?
Requirements: products, tools, prior knowledge.
Hardware
- 2800E-AND-S (OptixEdge 2800,Standard (ARM),None,FT Optix L (15 tokens),Standard AB,No Conformal Coat)
Software
- FactoryTalk Optix Studio Version 1.7.5.13
- FactoryTalk Optix Runtime Version 1.7.5.1
Previous Knowledge Required
Basic knowledge of installation, configuration and integration in:
- FactoryTalk Optix
- MQTT Protocol
- Industrial Networking
- Cybersecurity Fundamentals
Implementation Guide
This application works paired with the MQTT_Asset, showing data received via MQTT protocol in form of a control dashboard.
- Step 1
- Step 2
- Step 3
- Step 4
Download the Connected_Plant_Monitor.zip folder and extract its contents.
Install FactoryTalk Optix Studio and FactoryTalk Optix Runtime from FactoryTalk Hub.
Start the MQTT_Asset
connected-plant-monitor_MQTT_Asset folder_1.png
After that, open this project on another FT Optix window and run the application with FT Optix Emulator.
connected-plant-monitor_FactoryTalk Emulator_3.png
If the connection with the MQTT_Asset is working, the “Live Data” LED will be green.
connected-plant-monitor_LiveData_4.png
The data exchange is based on a Runtime Netlogic which can be found in the Netlogic folder. The Netlogic MQTTBrokerLogic is present on both applications but is configured differently.
The data exchange is based on a Runtime Netlogic which can be found in the Netlogic folder. The Netlogic MQTTBrokerLogic is present on both applications but is configured differently.
connected-plant-monitor_MQTTBrokerLogic MQTT_Asset_5.png
Connected Plant Monitor
Version 1.0 - October 2026