View the Lock for Update Logs
On the System Update tab of the RMCT, you can view logs for the following events:
- System update lock attempts
- Locked switchover attempts
Lock for Update Logs

Parameter | Description |
|---|---|
Event No. | A unique, sequential number to identify the event. |
Time Stamp | The date and time that the event was logged. |
Event Class | All events related to system update lock attempts have the same event class: Lock for Update log |
Basic Info | One of the following basic descriptions of the event:
If a system update lock attempt failed, refer to the Extended Info parameters to identify the cause. |
Extended Info 1 Extended Info 2 | Additional information that is related to the basic description of the event. Use this information to troubleshoot failed lock attempts. Possible causes include the following:
Extended information is not available for every event. |
Parameter | Description |
|---|---|
Event No. | A unique, sequential number to identify the event. |
Time Stamp | The date and time that the event was logged. |
Event Class | All events related to locked switchover attempts have the same event class: Locked Switchover log |
Basic Info | One of the following basic descriptions of the event:
If a locked switchover attempt failed, refer to the Extended Info parameters to identify the cause. |
Extended Info 1 Extended Info 2 | Additional information that is related to the basic description of the event. Use this information to troubleshoot failed locked switchover attempts. Possible causes include the following:
Extended information is not available for every event. |
Provide Feedback