Allen-Bradley, ControlFLASH Plus, ControlLogix, ControlLogix-XT, DH+, expanding human possibility, FactoryTalk, FLEX, FLEX 5000, FLEXHA 5000, GuardLogix, Integrated Architecture, Logix 5000, FactoryTalk Optix, OptixPanel, PanelView, PhaseManager, PlantPAx, POINT I/O, PointMax, Rockwell Automation, SequenceManager, Stratix, Studio 5000 Logix Designer, and VersaView are trademarks of Rockwell Automation, Inc.
CIP, CIP Safety, CIP Security, CIP Sync, ControlNet, DeviceNet, and EtherNet/IP are trademarks of ODVA, Inc.
microSD is a trademark of SD-3C.
Microsoft and Windows are trademarks of Microsoft Corporation.
Trademarks not belonging to Rockwell Automation are property of their respective companies.
Provide Feedback