Abort System Lock
To stop a system lock already initiated with the Lock for Update command, use the Abort System Lock command. The command is available as soon as you initiate a lock. When you select Abort System Lock, the following occurs:
- The redundant chassis status returns to Primary with Disqualified Secondary.
- The system update stops and the program in the secondary controller clears.
If you select Abort System Lock, you must download the program to the secondary controller before you can attempt a Lock for Update again.
Provide Feedback