Output Operation

FLEX 5000®
safety output modules can be configured with single or dual point operation types:
  • A single point operation type allows the outputs to turn on and off individually and to fault independently.
  • A dual point operation type verifies that safety task logic operates both outputs as a pair. If one output has a module fault, the other output goes to the safe state.
IMPORTANT: The point operation type affects the safety rating of the module.
Output Points Operation Types
Output Points Operation Types
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal