Inhibit a Device
You cannot inhibit or uninhibit safety I/O devices under these conditions:
- The application program is safety-locked
- A safety signature exists
Anytime necessary, you can programmatically inhibit and uninhibit with SSV from the standard task:
- Class Name: Module
- Attribute Name: Mode
- Source: Inhibit = 4; Uninhibit = 0
To inhibit a device, follow these steps.
- Select the device and then select Properties.
- In the navigation pane, select Connection.
- On the Connection view, select Inhibit Module and click Apply.The device is inhibited when the Inhibit Module checkbox is selected. If a communication device is inhibited, all downstream devices are also inhibited.
Provide Feedback