Safety Reaction Times
The input reaction time is the time from when the signal changes on an input terminal to when safety data is sent to the controller.
The output reaction time is the time from when safety data is received from the controller to when the output terminal changes state.
For information on how to determine the input and output reaction times, see the product documentation for your specific safety I/O device.
Provide Feedback