Logix SIS Safety Data

Use the following information to determine probability of a dangerous failure on demand (PFD) and average frequency of a dangerous failure per hour (PFH) values. These values apply to
GuardLogix®
5580 controllers in a Logix SIS 1oo2 SIL 3 system.

Useful Life

The useful life of safety controllers is 20 years.

Safety Data

For safety I/O devices safety data, including PFD and PFH values, see the manuals for those products.

Product Failure Rates

For a mean repair time (MRT) of 72 hours, use the safety calculations in the following table.
Safety Calculations
Attribute
MRT = 72 hr
PFH
1.367E-10
PFD
avg
(20 yr)
1.923E-05
Assumptions for safety calculations:
  • Component failure rates are constant over the life of the product.
  • Within the specified useful life (20 years), no proof test is needed.
IMPORTANT: To minimize system degradation during repair time, use the shortest MRT possible for your application. Exceeding an MRT of 72 hours is not recommended. If you can justify an MRT longer than 72 hours for your application, then you must use the formulas below to compute PFD
avg
and PFH.
For an MRT other than 72 hours, use the following PFD and PFH formulas to calculate PFD
avg
or PFH. Repair time is included in the calculations.
PFD and PFH Formulas
IMPORTANT: These calculations use assumptions that become invalid when the MRT value gets too large. The maximum MRT value permitted for SIL 3 safety functions in Logix SIS is 730 hours.
Safety Parameters
Parameter
Value
Description
λ
DU
6.40 x 10
-9
hr
-1
Dangerous undetected failure rate of a single controller
λ
DD
6.54 x 10
-7
hr
-1
Dangerous detected failure rate of a single controller
λ
S
6.61 x 10
-7
hr
-1
Safe failure rate of a single controller
λ
NPED
2.58 x 10
-6
hr
-1
No part/effect detected failure rate of a single controller
λ
Det
3.895 x 10
-6
hr
-1
Total detected failure rate of a single controller (λ
DD
+λ
S
+λ
NPED
)
T
≤ 20 years (17,5200 hours)
Mission time
Mission time is the length of time over which the device maintains the stated PFD, PFH, and λ ratings before replacement is required.
T
D
< SRT
Diagnostic test interval
β
2%
Common cause percentage
HFT
11
Hardware fault tolerance
The hardware fault tolerance equals
n
, where
n
+1 faults could cause the loss of the safety function. An HFT of 1 means that 2 faults are required before safety is lost.
LORF
7.61 x 10
-6
Loss of redundancy factor
MRT
[User-defined value]
Mean repair time for a failed controller
SC
3
Systematic capability
Systematic capability is defined in IEC 61508-4 as the confidence that the systematic safety integrity meets the requirements of the specified SIL rating.
1 When a controller chassis fails, the safety function continues to function with a HFT of 0 unit until the controller chassis synchronize.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal