Archive Safety Signature Reports for Audit
You can compare an original Safety Signature report to an updated Safety Signature report to show which elements changed and which elements did not change for auditing purposes. If your validation plan does not require revalidation of unchanged elements, your certification effort can be reduced, such as in these scenarios:
- You want to migrate a validated safety application to a future release without revalidating the entire application.
- You want to add or update some elements of a validated safety application without revalidating the unchanged elements.
- You want to copy some validated elements to another project without revalidating the copied elements.
Safety Signature reports are archived as .htm files in the following default directory:
C:\Users\Public\Documents\Rockwell Automation\Studio 5000\Logix Designer\Safety Signature Reports
Provide Feedback