Safety I/O Configuration Variations

As the range of products using the
CIP Safety
protocol continues to expand, there are variations to the typical safety I/O configuration steps. Product specific procedures and requirements can include the following:
  • Reset of ownership
  • Setting the safety network number (SNN)
  • Configuration signature generation
  • Request packet interval (RPI) limits
  • Device-specific configuration settings
For more information, see the user manual for your I/O device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal