Force Data

All data that is contained in an I/O, produced, or consumed safety tag, including CONNECTION_STATUS, can be forced while the project is safety-unlocked and no safety signature exists.
However, forces must be removed, not just disabled, on all safety tags before the safety project can be safety-locked or a safety signature can be generated. You cannot force safety tags while the project is safety-locked or when a safety signature exists.
TIP: You can install and remove forces on standard tags regardless of the safety-locked or safety-unlocked state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal