Configure the Safety Input Module Delay Time

To configure input module delay time in the Logix Designer application, follow these steps.
  1. In the configuration tree, right-click the safety input module and select Properties.
  2. In the navigation pane, select Points.
  3. Adjust the input delay time as required for your application.
Input Delay Time
Input Delay Time
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal