GuardLogix Architecture
The following examples of SIL 3 and SIL 2 systems show these features:
- The overall safety function
- TheGuardLogix®portion of the overall safety function
- How other devices that operate outside the safety function, such as HMI, are connected
Example SIL 3 System
Example SIL 2 System
Provide Feedback