GuardLogix Communication on a DeviceNet Network

DeviceNet®
bridges let the
GuardLogix®
controller control and exchange safety data with safety I/O modules on a
DeviceNet®
network.
GuardLogix 5580 Communication via a DeviceNet Bridge
GuardLogix 5580 Communication via a DeviceNet Bridge
Compact GuardLogix®
5380 controllers can communicate with safety devices on a
DeviceNet®
network via a 1788-EN2DNR
EtherNet/IP
to
DeviceNet®
linking device.
Compact GuardLogix 5380 Controller with a DeviceNet Network
Compact GuardLogix 5380 Controller with a DeviceNet Network
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal