800F-INT and 800F-INT-L Communication Interface Modules Status Indicators
See the status indicators
on your device to identify its status.
800F-INT and 800F-INT-L Communication Interface Modules Status Indicators
Status Indicator | State | Description |
|---|---|---|
MNS Module and EtherNet/IP™ In-cabinet network status | Off | The device is powered off or powered on, but with no IP address configured. |
Flashing Green | The IP address is configured for the device, but there are no connections. | |
Steady Green | The IP address is configured for the device, at least 1 connection is
established, and the bus is operating properly. | |
Flashing Red | The IP address for the device is configured, but an I/O connection has timed out,
a peer connection has timed out, the 800F operator is detached, or a major
recoverable fault exists. | |
Steady Red | A device on the bus has the same IP address or the internal diagnostics has
created a non-resettable fault. IMPORTANT: If a duplicate IP address fault is not present and the fault
persists through power cycles, the device should be replaced. | |
Flashing Green and Red | The device is performing its power-up testing. |
Provide Feedback