Plan a Local Network (Bus) Architecture
The local network bus supports one gateway and as many as 39 additional devices. Follow these
guidelines as you plan a bus:
- Each end of the bus must be terminated. The gateway provides internal termination.
- The minimum separation between connectors is 50 mm (1.97 in), but a 100 mm (3.94 in) or larger separation between connectors is recommended.
- The maximum network distance from the gateway connection to the 1486-CON-T1 terminator connection is 25 m (82 ft).
The figure below provides an example layout of a gateway with supported devices where
position 0 is the gateway, position 1…21 are the supported devices, and position 22 is the
1486-CON-T1 terminator.
Example of Gateway and Supported Devices
Provide Feedback