Import/Paste Configuration dialog - Routines tab

Use this dialog to view routine definitions. All settings in this dialog are read-only and cannot be changed.
TIP: To open the Import/Paste Configuration dialog - Routines tab:
  1. Select
    File > Import Component > <component>
    .
  2. Select a component for import and select
    Open
    .
  3. On the
    Import Content
    pane, select
    Routines
    .
The dialog lists information for imported routines from a program,
Equipment Phase
, or Add-On Instruction, and for the Diagram routine from an imported
Equipment Sequence
. When you select
Routines
in the
Import Content
pane, the routine definitions grid view displays in the Details pane. The routine definitions grid contains the union of all the routines that appear in both the import content and the project, and shows the disposition of each. For example, if a routine exists in the program in the project, but does not exist in the program being imported, the operation for that routine is set to
Delete
.
The
Operation
setting for these routines is based on the Operation chosen for the component being imported.
The routines item does not display if:
  • The Add-On Instruction of which it is a part is protected and not viewable.
  • Collides with an Add-On Instruction in the project that is protected and not viewable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal