PMTR time settings
Use the
Time configuration
tab on the PMTR Properties
dialog box to configure time parameters for Process Motor (PMTR) instructions.To configure time settings for PMTR instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- UnderAdvanced, selectTime configuration.
- Configure these settings:
- Delay with contactors open when changing speed or direction. Enter the number of seconds to pause, with contactors open, when the motor changes speed or direction.
- Feedback delay for loopback test or when feedback not used.Enter the number of seconds to delay feedback for a loopback test or when the feedback is not used. Use this setting to configure a virtual feedback time.
- Time after start for feedback before fault. Enter the number of seconds to allow motor run feedback to show running after a start command. If run feedback does not show that the motor started, the instruction reports aFail to Startstatus.
- Time after stop for feedback before fault. Enter the number of seconds to allow motor run feedback to show stopped after a stop command. If run feedback does not show the motor stopped, the instruction reports aFail to Stopstatus.
- Time to pulse Out_Reset to clear fault. Enter the number of seconds to pulse the output that requests to clear the motor fault.
- Maximum jog time. Enter the maximum number of seconds to jog the motor before the jog command automatically clears. If this value is zero, the jog time is unlimited; the instruction does not automatically clear the jog command, and jogging continues until the commanding source (such as the operator faceplate) clears the jog command.
- Time to sound audible on commanded start. Enter the number of seconds to sound an audible notification when the motor is commanded to start.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state, such asRunning,Stopped, orOut of service.
- Device issues. Displays fault conditions, such asFail to startorConfiguration error.
- SelectApply.
Provide Feedback