HMI CV label information for PFO
Use the
CV label
tab of the PFO Properties
dialog box to enter the information provided by the selected PFO instruction or function block to label HMI faceplates.To enter HMI CV label information for PFO instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select the arrow next toHMIand then selectCV Label.
- Set the parameters:
- Output CV label. Type the label to show on the graphic HMI faceplate for the output.
- EU. Text for engineering units (CV) to be displayed on HMI.
- View the read-only parameters:
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Off, Pulse on, or Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Feedback fault or I/O fault.
- SelectApply.
Provide Feedback