PAO HMI device state labels
Use the
HMI State configuration
tab on the PAO Properties
dialog box to configure device state labels for Process Analog Output (PAO) instructions.To configure HMI device state labels for PAO instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select the arrow next toHMIand then selectState configuration.
- Set the parameters:
- Target state labels. Type the label to display for the device target state.
- Transition state labels. Type the label to display for the device transition state.
- View the read-only parameters:
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Off, Pulse on, or Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Feedback fault or I/O fault.
- SelectApply.
Provide Feedback