Other
Data exchange support for other devices:
Other
Catalog Number or Product Family | RDF support | AML support |
|---|---|---|
Logix Designer projects | Partial 1 | Partial 1 |
Generic switches | Yes | Yes |
Ethernet switches - Generic | Yes | Yes |
Generic computers | Partial 2 | Partial 2 |
PanelView Plus graphic terminals | Yes | Yes |
MobileView mobile terminals | Yes | Yes |
FactoryTalk View applications or servers | No | No |
Graphics | No | No |
Files | No | No |
Text Boxes | No | No |
Shapes | No | No |
Links | No | No |
Combination Generator Control Module | No | No |
Combination Generator Control Module, 2-Port | No | No |
Powermonitor1000 | No | No |
1557... | No | No |
20-COMM-E | Yes 3 | Yes 3 |
22-COMM-E | Yes 3 | Yes 3 |
2706-PENETX | No | No |
440C-CR30-22BBB | No | No |
CEP7-ETN | No | No |
CIP-MODULE | No | No |
DEVICENET-SAFETYMODULE | No | No |
DPI-DRIVE-PERIPHERAL-MODULE | No | No |
DSI-DRIVE-PERIPHERAL_MODULE | No | No |
Emulate 5570 | No | No |
ETHERNET-SAFETYMODULE | No | No |
ETHERNET-SAFETY-STANDARD-MODULE | No | No |
FLEX_MODULE | No | No |
Generic Computer | Yes 4 | Yes 4 |
Generic Switch | Yes 5 | Yes 5 |
L2yEmbedded Analog_IO | Yes 6 | Yes 6 |
L2yEmbedded Counters | Yes 7 | Yes 7 |
L2yEmbedded Discrete_IO | Yes 8 | Yes 8 |
Logix Block | No | No |
MDCOMM-ENET | No | No |
RHINOBP-DRIVE-PERIPHERAL-MODULE | Yes 3 | Yes 3 |
RIO-MODULE | No | No |
RSLinx | No | No |
SCANport-DRIVE-PERIPHERAL-MODULE | No | No |
VersaView CE* | No | No |
Other Networks | Yes | No |
1 Project must not include any unsupported devices. Data imported subject to the limitations on included devices.2 The computer name property of the generic computer object not supported for AML export or import. Assigns a default name to the generic computer object during import that can be updated after the import is complete.3 PowerFlex peripheral.4 Computer ignored.5 Connections only.6 As 1.10.1647 As 1.109.718 AS 1.7.64 | ||
Provide Feedback