Export an Equipment Sequence

Export an Equipment Sequence so you can import the sequence into another project, or to create a backup copy of a sequence while you modify the original.
To export an equipment sequence:
  1. In the
    Controller Organizer
    or the
    Logical Organizer
    , select the Equipment Sequence that you want to export.
  2. Right-click the Equipment Sequence and select
    Export Equipment Sequence
    .
  3. In the
    Export Sequence
    dialog box, click
    Export
    .
    You can also select a destination for the exported file, modify the file name, and add a description for the file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal