Nonvolatile Memory Load/Store dialog box
Use the
Nonvolatile Memory Load/Store
dialog box to:- View the current and stored controller image.
- Store a project in memory card.
- Load a project from the memory card.
- Enable Firmware Supervisor to automatically load firmware when you replace a device in the system.
- If a safety application is stored on the card, view the safety-lock status and safety task signature.TIP:When you open this dialog box, theLogix Designerapplication locks the controller so other users can not interrupt your load or store operation.
TIP:
To open the Nonvolatile Memory Load/Store dialog:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click theNonvolatile Memorytab, and clickLoad/Store.
Parameters | Description |
Image in Nonvolatile Memory | Parameters pertaining to the image stored in nonvolatile memory on the controller. |
Controller | Parameters pertaining to the current image in the controller. |
Name | The name of the stored controller image that resides in nonvolatile memory or the project that resides in controller memory. |
Type | Name of the controller. |
Revision | The firmware revision. In order for the image in nonvolatile memory to be loaded back into controller memory, the firmware revision of that image must match the revision of the controller. |
Load Image | The condition under which the image stored in nonvolatile memory is loaded back to controller memory.
|
Load Mode | The mode the controller enters upon loading from nonvolatile memory. This parameter is unavailable when Load Image is set to User Initiated .
The Load Mode only applies if the controller keyswitch is in the remote position when loading. If the controller keyswitch is in Run or Program, the controller will return to that mode once the load is complete. The controller key switch always has priority over the Load Mode . |
Safety Application | The nonvolatile memory safety lock status (locked or unlocked). This parameter is available when you are online or connected with a controller that has a nonvolatile memory card containing a Safety controller application. |
Safety Signature | The nonvolatile memory Safety task signature status (ID, Date, and Time). Tip:
Compact GuardLogix 5380 and GuardLogix 5580 controllers![]() This parameter is available when you are online or connected to a controller with a nonvolatile memory card that contains a Safety controller application. An Information icon appears if there is a status message to display. |
![]() | Opens the Safety Signature ID dialog box to view and copy the entire 32 byte ID for Compact GuardLogix 5380 and GuardLogix 5580 controllers.Compact GuardLogix 5380 or GuardLogix 5580 controller |
Image Note | Descriptive information about the image stored in nonvolatile memory. You may enter up to 128 text characters. |
Automatic Firmware Update | Also referred to as Firmware Supervisor. Allows automatic firmware updates to modules in the I/O Configuration Tree that have electronic keying set to Exact Match.
Tip: Firmware Supervisor only supports firmware with the NVS and BIN file format. Starting in December 2015, firmware for modules may be provided in a new Device Management Kit (DMK) file format, for example, 1756-L73_28.011.dmk. To use Firmware Supervisor with hardware modules whose firmware is provided in a DMK file format, you must first extract the NVS and BIN files from the DMK using the DMK Extraction Tool that is installed with ControlFLASH v13.00. Refer to the ControlFLASH online help for instructions on how to use the DMK Extraction Tool. |
Stored | The date and time the image was stored in nonvolatile memory. |
Load | Opens the Load dialog box to load the nonvolatile memory image into controller memory. This button is unavailable when:
|
Store | Opens the Store dialog box to store the controller memory to nonvolatile memory. This button is unavailable when:
|
Status Bar | Shows the reason the Load and Store buttons are unavailable. Only shows one status at a time. |
Provide Feedback