Open Project from Source Control Dialog Box
Use this dialog box to open a project from source control.
Parameters
Parameter | Description |
|---|---|
Look in: | Select the directory in the AssetCentre archive in which the project to open or import resides. (the last open location is remembered upon subsequent returns.) |
Up One Level - ![]() | Move up one level in the directory tree. Active when logged in to a server or database and not already at the top level of the tree. |
View Menu - ![]() | Select the view type (list of file names or a list of file names with the username). Active when logged in to a server or database. |
Login - ![]() | Log in to a specific server and attach to a specific database. |
Select Version or Label for the Operation - ![]() | Select an archived element based on either version or a label. Active when a file is selected. |
Help - ![]() | View help on how to use source control. |
Directory/File | Displays the directories and files contained within a specific server or database. View Menu determines the view type (list or details). |
Check Out | If unselected, retrieves a copy of the selected file when selecting Get .If selected, checks out the retrieved file. If the selected file is checked out. option is not selected or active |
File Name | Displays the currently selected file (read-only) |
Files of type | Choose the type of file to open or import (ACD file is the only option). |
Get | Retrieve (get) file or check out the file (if Check Out is selected). Active when logged in to a server or database and if a file selected to retrieve. |
Cancel | Cancel the open or import and close the Open/Import Project dialog box. |
Help | View Help on the Open/Import Project dialog box. |
Provide Feedback