Driver and Path Configuration dialog box settings

Use the
Drive and Path Configuration
dialog box to manually enter a communications driver and path. The following are the
Driver and Path Configuration
dialog box settings:
TIP:
  • Configure ControlNet and DH+ drivers in the <RSLC> user interface or in the
    FactoryTalk Administration Console
    for
    FactoryTalk Linx
    .
  • Manually-entered drivers and paths do not appear in the
    Who Active
    dialog box. Drivers and paths appear wherever the current path normally displays, with the driver and path concatenated, such as AB_KTC-1\2,6,1,0.
Setting
Description
Driver
Used to select from the list of running drivers in the communication software edition.
Path
Enter the CIP path to a controller that
Logix Designer
uses when executing a
Go Online
,
Upload
, or
Download
command. The path also writes to any project.
NOTE:
For
ControlNet
and
DH+
, construct the path starting from the communications module in the local chassis. Separate the number or addresses entered in each step with a comma. All numbers are decimal, by default. Enter any number other than an Ethernet/IP address in another base by using an IEC-1131 prefix ("8#" for octal, "16#" for hexadecimal). Ethernet/IP addresses are always dot-separated decimal numbers.
Recent
Navigates to the
Select Recent Communications Path
dialog box, and select a recent saved path as the current communications path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal