Develop a solution for importing UI
    Use OPC UA communication to import the UI from another project and display the values of selected variables.
Application example (server and client)

     TIP: 
    
Download a sample project:
 ImportUI.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
     TIP: 
    The Client project imports data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
Application design example (server and client)

Select  to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
  to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
Run
Provide Feedback