Develop a solution for importing translations
    Use OPC UA communication to import translations from another project.
Application example - client, login form

Application example - client, logged in Italian user

Application example - client, logged-in American user

     NOTE: 
    
Download a sample project:
 ImportTranslations.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
     TIP: 
    The Client project imports data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
  to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
Run
Provide Feedback