Develop a solution for importing objects
    This design-time script creates objects in the project based on the data from a 
CSV
 file.
     TIP: 
    
You can download a sample project from:
 ObjectsFromCSV.zipPrerequisites
In the following example, the 
    
CSV
 file contains information about alarms and model variables used by these alarms.
        variable,var1,boolean variable,var2,uint32 alarm,alarm1,digital,var alarm,alarm2,analog,var2
| #1 column | #2 column | #3 column | #4 column | 
|---|---|---|---|
| Indicates whether you need to create a project variable (keyword  variable) or an alarm (keyword alarm). | Indicates the name of the node to be created. | Indicates the datatype to use to create the variable:
                     
 | Indicates the variable to point the alarm to. | 
     TIP: 
    The 
CSV
 file is a part of the sample project. You can also download the CSV
 file individually from: alarms.csv- To develop the project
- Save the project.
Provide Feedback