Develop a contact form
    Develop a contact form that sends emails to a predefined address.
Application example

     TIP: 
    
You can download a sample project from:
 ContactForm.zipPrerequisites
- To develop the project
- Save the project.
Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback