Develop a button that changes label text
    Develop a button that changes the text of a label when you select the button.
Application example


     TIP: 
    
You can download a sample project from:
ButtonThatChangesLabelText.zipPrerequisites
- To develop the project
- Save the project.
Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback