Create a linear gauge
    Create a linear gauge that shows the temperature.
- InProperties, right-clickMainWindow (type)and select .
- InProperties, set theEditablevariable value toFalse.
- Create a variable:- InProperties, at the top, selectand select Analog variable. Analog variable.
- Create a complex dynamic link between theAnalogVariable1property and the actualAnalogVariable1variable by using binding mode.  - DynamicLink
- EU Mode
- Localize.
 
 
- Create a dynamic link betweenLow limitand
- Create a dynamic link betweenHigh limitand
- SetConstraintoTrue.
 For more information about dynamic links, see Create dynamic links.
- Link the variable alias:- InProperties, create a dynamic link betweenValueand .
- Create a dynamic link betweenMinimum valueand .
- Create a dynamic link betweenMaximum valueand .
 For more information about dynamic links, see Create dynamic links.
Provide Feedback