Create a label
    Create a label that displays temperature in a format adjusted to the locale of a logged-in user.
- InProject viewpane, right-clickMainWindow (type)and select .
- Create a label variable:- InProperties, at the top, selectand select Analog variable. Analog variable.
- Create a complex dynamic link between theAnalogVariable1property and the actualAnalogVariable1variable by using .  - DynamicLink
- Configure
 
 
 
- Create a complex dynamic link between theTextandAnalogVariable1with the use of a string formatter:  - StringFormatter1
- {0} {1}- {0} DynamicLink
- {1} DynamicLink
 
 For more information about dynamic links, see Create dynamic links.
Provide Feedback