Create an acceleration gauge and labels
    - Create the speed gauge:- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the gauge, select, and enter AccelerationGauge. AccelerationGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
 
- Create the speed label:- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enter AccelerationLabel. AccelerationLabel.
- InProperties, setTexttoAcceleration.
 
- Create the speed value label:- InProject view, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enter AccelerationValueLabel. AccelerationValueLabel.
- InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
 
Provide Feedback