Develop a temperature change alarm
    Develop an alarm that signals when temperature exceeds a set value.
Application example

     NOTE: 
    
Download a sample project:
 TemperatureChangeAlarm.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback