Configure a recipes editor
    Configure the recipes editor to manage recipes at runtime.
- From the toolbar, select.Template Libraries
- InLibraries, search forRecipes Editor.
- UnderComponents, dragRecipes EditorontoPage4 (type)inProject view.
- SelectClose.
- InProject view, selectRecipesEditor1.
- InProperties, setHorizontal alignmenttoStretch.The object adjusts its width to the container at runtime.
- InProject view, selectRecipesEditor1.
- InProperties, create a dynamic link betweenRecipeSchemaand .For more information about dynamic links, see Create dynamic links.
- Right-clickRecipesEditor1and selectExecute Setup.
Provide Feedback