Configure a digital alarm
    Configure a simple Boolean alarm that warns you about issues with Motor1 at runtime.
     TIP: 
    By default, a digital alarm triggers when its 
Input variable
 equals to 1.- InProject view, right-clickAlarmsand select .
- InProperties, create a dynamic link between theInput variableandMotor1Alarmvariable.For more information about dynamic links, see Create dynamic links.
- InMessage, enter a warning message.For example, enterMotor1 alarm.
Provide Feedback