Project view
    Project view
 displays the contents of the FactoryTalk Optix Application
 in a tree structure of folders.Folders
      Each folder has a dedicated icon and context menu. The context menu displays objects that you can create in that folder. Any subfolder that you create displays the same options as the folder on which it is based. You can create multiple versions of a folder.
Buttons
      Project view
 contains buttons for navigating the contents of the application. Some buttons appear on either the title bar of Project view
 or in the selected object.
        
  | Item | Description | 
|---|---|
|   Navigate backward | Set focus on the previously selected pane. | 
|   Navigate forward | Set focus on the next selected pane. | 
|   Split project view | Divide  Project view into two panes. | 
|  Add new | Create a node inside the selected node. | 
| Delete | Remove the selected node and the nodes that it contains. | 
|   Detach view | Detach the pane from the main window. | 
|   Attach view | Detach the pane to the main window. | 
|   Lock | Lock the selected child node to hide it from  Project view. You cannot edit locked child nodes. | 
|   Unlock | Unlock the selected child nodes to display it in  Project view. You can edit unlocked child nodes. | 
|  | Open the selected object in the dedicated editor. Only certain object types have a dedicated editor.  | 
Search bar
      Use 
        
  Search
 in Project view
 to search for and filter project nodes in the tree structure.| Item | Description | 
|---|---|
| Search | Filters the project nodes in the tree structure based on the search query. | 
|  | Displays if you enter a search query. Select to clear the search query. | 
|  | Expands the available filters picker. | 
|  | Collapses the available filters picker. | 
|  | Indicates active filters. Expand or collapse the available filters picker. | 
Provide Feedback