Main toolbar
    The main toolbar at the top of 
FactoryTalk Optix Studio
 contains buttons used by all views in the software.| Item | Description | Function | 
|---|---|---|
|  | Project | Opens the Start page. The Start page allows you to create, open, or close a project. | 
| Save | Saves the project. Select an option from the list to: 
 | |
|  | Save and Commit | Saves changes and commit the changes to back them up in the local repository. | 
| Push to remote | Pushes saved and committed changes to the remote repository for users to see the latest changes to the project. | |
| Pull from remote | Pulls the latest changes from the remote repository to see the latest changes that other users have made. | |
|  | View History | Views the history of changes to the project. Restore any commit to revert to a previous version of the project. | 
| Undo | Cancels the last operation. | |
| Redo | Repeats the last operation. | |
| Browse project files | Opens the project resource window for displaying, importing, or deleting project files such as images, videos, documents, and certificates. | |
| Template Libraries | Opens the default and custom libraries and template variables.  | |
|  | Open .NET Solution | Opens the .NET project to incorporate additional functionality using custom C# code.  | 
| Open dashboard page | Opens a configuration dashboard to begin designing your user interface. Select the list to configure the connected device, data logging, and recipes, or manage users and groups. | |
|  | Stop | Stops the application that is running on the client device. | 
| Run on Emulator | Compiles, transfers, and runs the application on the selected client device or emulator. Select a different client device from the list.  | |
|  | VPN | Opens a VPN connection. | 
|  | Remote Desktop | Opens a Remote Desktop connection. | 
Provide Feedback