Third-party .NET libraries
    Extend the C# programming language capabilities using third-party .NET libraries.
     IMPORTANT: 
    
FactoryTalk Optix Studio
 supports only .NET libraries with the .NET Standard 6.0 destination framework.Add a third-party library in the editor of your choice. See Add a third-party library to the Visual Studio project and Add a third-party library to the Visual Studio Code project.
Provide Feedback