Field variables
    To reference field variables (controller tags or variables of an OPC UA server), use special project variables (tags) that report the value of the field variables.
     TIP: 
    When a tag variable is read, 
FactoryTalk Optix Studio
 reads the field variable and updates the value of the project variable. When a tag variable is written, FactoryTalk Optix Studio
 propagates the write on the field variable.Read/write field variables in FactoryTalk Optix Studio and in C#
      FactoryTalk Optix Studio
 and in C#Field variable reading/writing occurs automatically when a tag variable is read/written in 
    
    
FactoryTalk Optix Studio
. To reproduce the same behavior in C#, you must use specific APIs in these cases:
        - Reading/writing tag variables synchronized with corresponding controller tags.
- Reading/writing important variables with an OPC UA Client object from an OPC UA server to synchronize them with the OPC UA server corresponding variables.
- Reading/writing a variable directly or indirectly connected (using dynamic links or converters) to a variable described in previous cases.
     IMPORTANT: 
    When a tag variable is read using the 
Get
 method, FactoryTalk Optix Studio
 does not read the value on the field and can return a value that has not been updated.Value change events
      - To subscribe methods to the change value event of the field variables, use aRemoteVariableSynchronizerobject. TheRemoteVariableSynchronizerobject updates the project variables referring to the field, without repeating readings through simple API reading.
- TheRemoteVariableSynchronizerobject is not required if a link to a tag variable from a graphical object, data logger object, alarm or recipe schema object exists inFactoryTalk Optix Studio. In a NetLogic, you can subscribe the change value method directly to the linked tag variable.
- Management of communication delays with the field. If a field variable is read/written in NetLogic, execute the instructions, and verify that the current value is read or written. The APIs for reading/writing field variables are synchronous. Their execution must end before the next instruction can be ran.
Provide Feedback