Collections
     A collection is a C# object that contains multiple objects. You can use collections for counting, iterating, adding, and removing child nodes of a given node.
Generic children collections
      Available in every 
IUANode
 C# object and each project node. Generic children collect the object/node properties and other objects/nodes that are its direct children.Specialized collections 
      
  | Type of project object | BrowseNameof the object type | Collection | Type of collection object | 
|---|---|---|---|
| Data logger | DataLogger | VariablesToLog | VariableToLog | 
| Event logger | EventLogger | EventFields | EventField | 
| OPC UA Client | OPCUAClient | RuntimeConfigurations | RuntimeConfigurationEntry | 
| OPC UA Server | OPCUAServer | NodesToPublish | NodesToPublishConfigurationEntry | 
| NodesToPublish.Nodes | NodePointerthat point to the project nodes | ||
| NodesToPublish.Users | NodePointerthat point to users | ||
| Report | Report | Sections | UI.Item | 
| Retentivity database | RetentivityStorage | Nodes | IUAVariablethat point to the roots of the nodes with the retentivity set. | 
| Store | Store | Tables | Table | 
| Table | Table | Columns | Column | 
| Circular gauge | CircularGauge | WarningZones | WarningZone | 
| Linear gauge | LinearGauge | WarningZones | WarningZone | 
| Data grid | DataGrid | Columns | DataGridColumn | 
| Navigation panel | NavigationPanel | Panels | NavigationPanelItems | 
| Trend pen | Trend | Pens | TrendPen | 
| XY chart line | XYChart | Pens | XYChartPen | 
| Communication station | IStation | Tags | Tag | 
| TagStructure | CommunicationDriver.TagStructure | ||
| Containers Graphical objects that can have children | - | Items | Item | 
| Object | BaseObject | InstanceNodeCollection | BaseObject 
     TIP: 
    Instances of any derived types that are not represented in  InstanceNodeCollection. They can be listed manually with the derived types first. | 
| Variable | BaseVariable | InstanceNodeCollection | BaseVariable 
     TIP: 
    Instances of any derived types that are not represented in  InstanceNodeCollection. They can be listed manually with the derived types first. | 
Provide Feedback