LogicObject.SetAlias(string, IUANode)
    Sets the value of an alias, or the node the alias points to. 
void SetAlias(stringaliasName, IUANodepointedNode);
Arguments
      - aliasName(string)
- TheBrowseNameof the alias to set.
- pointedNode(IUANode)
- ANodeto which the alias must point to.
Example
      The following example shows the 
MotorInstance
 alias that points to the Motor1
 node.var myMotorInstance = Project.Current.FindObject("Motor1"); LogicObject.SetAlias("MotorInstance"), myMotorInstance);
Provide Feedback