LogicObject.GetPanelLoader(string)
    Returns a 
PanelLoader
 C# object that corresponds to the Dynamic panel
 object indicated in the argument.
     TIP: 
    The API uses the alias that the Presentation Engine automatically generates at runtime for the panel. See Aliases.
PanelLoader GetPanelLoader(stringpanelLoaderName);
Arguments
      - panelLoaderName(string)
- TheBrowseNameof theDynamic panelobject.
Returns
      - PanelLoader
- A C# object that corresponds to theDynamic panelobject.
Example
      The following example shows an API that returns a C# object that corresponds to the 
PanelLoader1
 object, in which you want to create a Motor
 object.var myPanel = LogicObject.GetPanelLoader("PanelLoader1"); var motor = InformationModel.MakeObject("Motor"); myPanel.ChangePanel("Panel1");
Provide Feedback