InformationModel.MakeAlias(browseName)
    Creates an alias and returns a corresponding 
IUAVariable
 C# object.static IUAVariable MakeAlias(QualifiedNamebrowseName);
Arguments
      - browseName(QualifiedName)
- TheBrowseNameof the new alias.
Returns
      - IUAVariable
- A C# object that corresponds to the project object created.
Example
      The following example shows an alias that is created in the 
Motor1
 object of the FactoryTalk Optix Studio
 project:var modelFolder = Project.Current.Get("Model"); var alias = InformationModel.MakeAlias("CurrentMotor"); modelFolder.Add(alias); modelFolder.SetAlias("Model", Project.Current.Find("Motor1"));
Provide Feedback