C# API reference
    Use C# APIs to create logics that manipulate project nodes, variables, log messages, dynamic links, aliases, paths, and translations.
The complete lists of tasks that can be used from the C# API reference include:
      
Provide Feedback