View changes to a project
    View the committed changes of the open project by viewing the project history.
In  represents a change that is committed to the local repository and
  represents a change that is committed to the local repository and  represents a change that is pushed to the remote repository. If you are not using version control on your computer, Configure version control to view project history in
  represents a change that is pushed to the remote repository. If you are not using version control on your computer, Configure version control to view project history in 
Version history
,  
 Local history
 
 Remote history
FactoryTalk Optix Studio
.- In the main toolbar of the open project, select. View history View history
- InVersion history, selectto select a commit. The changes in the commit appear highlighted. If the project is new, all content for the project is highlighted. 
- Expand a highlighted object to view the changes in the object.TIP: Values that change in an object are crossed out and an arrow points to the new value.
Provide Feedback